SFFS700 May 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
This mode will check the error signaling path of a lockstep compare error from the LCM to the error aggregator logic (e.g. NMIWD). This test can be executed at any time during the device operation when the lockstep comparator is enabled. Executing this test will result in assertion of the lockstep comparison error signal. There are separate configurations available to force a compare error to each of the redundant comparators. Once this mode is enabled, it will be active for only one cycle. Enabling the error forcing mode will cause the first functional output from the primary module to be inverted.
It is not possible to execute this test with the debugger connected since the lockstep comparator gets disabled with debugger connection.