SFFS809 September 2024 TLV710-Q1
This section provides a failure mode analysis (FMA) for the pins of the TLV710-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
Class | Failure Effects |
---|---|
A | Potential device damage that affects functionality. |
B | No device damage, but loss of functionality. |
C | No device damage, but performance degradation. |
D | No device damage, no impact to functionality or performance. |
Figure 4-1 shows the TLV710-Q1 pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TLV710-Q1 data sheet.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
EN1 | 1 | LDO 1 is always off due to EN being grounded. | B |
IN | 2 | Output voltage is at or near ground. | B |
EN2 | 3 | LDO 2 is always off due to EN being grounded. | B |
GND | 4 | No effect. Normal operation. | D |
OUT2 | 5 | Output voltage 2 is at or near ground. Device is in current limit. The device can cycle in and out of thermal shutdown depending on power dissipation. | B |
OUT1 | 6 | Output voltage 1 is at or near ground. Device is in current limit. The device can cycle in and out of thermal shutdown depending on power dissipation. | B |
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
EN1 | 1 | LDO is in unknown state. | B |
IN | 2 | No input to LDO. Output is at or near ground. | B |
EN2 | 3 | LDO is in unknown state. | B |
GND | 4 | There is no current loop for internal biasing; device cannot operate. | B |
OUT2 | 5 | Device 2 output is unregulated and the load is not powered. | B |
OUT1 | 6 | Device 1 output is unregulated and the load is not powered. | B |
Pin Name | Pin No. | Shorted to | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|---|
EN1 | 1 | IN | If EN is positive voltage above the IN absolute maximum rating, IN can be damaged. | A |
IN | 2 | EN2 | If EN is positive voltage above the IN absolute maximum rating, IN can be damaged. | A |
GND | 4 | OUT2 | Output voltage is at or near ground. Device is in current limit. The device can cycle in and out of thermal shutdown depending on power dissipation. | B |
OUT2 | 5 | OUT1 | Output voltage is driven to unknown voltage. High current drive between pins is possible leading to potential thermal shutdown. | A |
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
EN1 | 1 | If EN is positive voltage above the IN absolute maximum rating, IN can be damaged. | A |
IN | 2 | No effect. Normal operation. | D |
EN2 | 3 | If EN is positive voltage above the IN absolute maximum rating, IN can be damaged. | A |
GND | 4 | Output voltage is at or near ground. | B |
OUT2 | 5 | Regulation for LDO 2 is not possible. The output voltage equals input voltage. | B |
OUT1 | 6 | Regulation for LDO 1 is not possible. The output voltage equals input voltage. | B |