SFFS889 July 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
The controller area network (DCAN) interface provides medium throughput networking, with event based triggering, compliant to the CAN protocol. The DCAN modules require an external transceiver to operate on the CAN network. The following tests can be applied as diagnostics for this module (to provide diagnostic coverage on a specific function):
The following tests can be applied as a test-for-diagnostic on this module: