SLAA202B February 2005 – December 2018 MSP430F149 , MSP430F149 , MSP430F2252-Q1 , MSP430F2252-Q1 , MSP430F2272-Q1 , MSP430F2272-Q1 , MSP430F2274 , MSP430F2274 , MSP430FG4619 , MSP430FG4619
The implementation of the IrLMP layer was accomplished by following the specifications of the IrDA Lite documentation. The main task of this layer is to verify that the DLSAP-SEL and SLSAP-SEL values are correct and that the correct service is using them. It also verifies that the services requested by the peer are supported as specified in the GetValueByClass function. Finally, it provides the frame format that carries the data to be exchanged by the two devices.