SLAA249B April 2005 – September 2018 MSP430F169 , MSP430F169 , MSP430F5252 , MSP430F5252 , MSP430F5253 , MSP430F5253 , MSP430F5254 , MSP430F5254 , MSP430F5255 , MSP430F5255 , MSP430F5256 , MSP430F5256 , MSP430F5257 , MSP430F5257 , MSP430F5258 , MSP430F5258 , MSP430F5259 , MSP430F5259
This is the slave code source used with msp430x26x_SMB_mstr_PEC.c. The example writes one byte of data and one byte of PEC from the slave. The PEC byte is calculated using a CRC-8 algorithm on the transmitted byte and slave address. An improved and more efficient CRC-8 algorithm is used.