SLAA381C December 2007 – September 2018 MSP430F233 , MSP430F235 , MSP430F2410 , MSP430F247 , MSP430F248 , MSP430F249
For the MSP430™ MCUs, the maximum frequency at which the CPU can operate depends on the supply voltage. This specification can be found in the recommended operating conditions of each device-specific data sheet. In general, it can be said that this specification differs for the F13x/F14x and F23x/F24x families of microcontrollers. However, an F23x/F24x MCU can always operate under the same operating conditions in terms of supply voltage and CPU clock frequency (MCLK) as an F13x/F14x MCU. If a designer who migrates an existing design to an F23x/F24x MCU wants to take advantage of the increased maximum clock frequency, it is important to closely review the recommended operating conditions in the F23x/F24x MCU data sheet. [4]
It is of extreme importance that this relationship is also observed during power-ramp scenarios. Violating this maximum frequency and voltage dependency can result in unpredictable code execution. Note that F23x/F24x MCUs have a built-in SVS module that can ensure that this operating condition is not violated.