SLAA450G April 2010 – April 2020
The existing BSL software can easily be ported to a different communication interface. This is possible because the Peripheral Interface code that handles communication is very loosely tied to the rest of the BSL software. To implement a custom Peripheral Interface, the following functions in the file BSL430_PI.h must be defined.