SLAA450G April 2010 – April 2020
After power up, the device first checks the BSL signature. If the appropriate values are found, the device calls the BSL protect function. The BSL protect function is described in detail in Section 1.2.1, but its main responsibilities are to secure the BSL memory and to indicate if the BSL should be started instead of the user application. The device start-up sequence occurs according to the flow chart in Figure 1.