SLAA450G April 2010 – April 2020
This is a custom linker command file that places the project code output into the BSL memory locations. In addition, it has definitions for the reserved BSL memory sections described previously. In general, it should not need modification. In some BSL linker command files, the reset vector output is intentionally placed out of the correct device RESET vector location, as this would cause the device to continually try to jump into the protected BSL memory, which would cause a reset, and thus an infinite reset loop.