SLAA517F May 2012 – August 2021 MSP430F6720A , MSP430F6720A , MSP430F6721A , MSP430F6721A , MSP430F6723A , MSP430F6723A , MSP430F6724A , MSP430F6724A , MSP430F6725A , MSP430F6725A , MSP430F6726A , MSP430F6726A , MSP430F6730A , MSP430F6730A , MSP430F6731A , MSP430F6731A , MSP430F6733A , MSP430F6733A , MSP430F6734A , MSP430F6734A , MSP430F6735A , MSP430F6735A , MSP430F6736 , MSP430F6736 , MSP430F6736A , MSP430F6736A
If the procedures and configurations are complete in the previous two sections, the results can be observed and based on these; calibration can be performed. Calibration is key to any meter’s performance and is absolutely necessary for every meter to go through this process. Initially every meter would exhibit different accuracies due to silicon-silicon differences, sensor accuracies and other passive tolerances. To nullify their effects, every meter should be calibrated. Simple procedures to accomplish this process are shown in this section. For any calibration to be performed accurately there should be an accurate source available. The source should be able to generate any desired voltage, current and phase shifts (between V and I) or power factors. In addition to an accurate source, there should also be a reference meter that acts as an arbitrator between the source and the meter being calibrated. This section discusses a simple and effective method of calibration of this 1-phase EVM.
A PC GUI is included in the file that can be downloaded from the One-Phase Metrology with Enhanced ESD Protection Reference Design.