SLAA600E June 2013 – January 2024
When using MSPBootProjectCreator, several files require user modification after their creation. These files include:
The portions of these files that need to be modified are marked with the //TODO: tag that is easily searchable and stands out in CCS. Each TODO also shows up in the CCS task list, which can be accessed through View → Other... → General → Tasks. Each task includes instructions on what must be modified and where to look for examples. This modification is required for proper operation of MSPBoot and application code when using the project generation script.