SLAA600E June 2013 – January 2024
There is one TODO item in TI_MSPBoot_AppMgr.c that require user modification. In the TI_MSPBoot_Restore_DefaultClockSettings function, it is recommended that the user set the clock settings to default as if the part had just reset. This function is called just before jumping to the application code and will ensure that the MSPBoot clock settings are not carried over to the application.