SLAA638A august 2014 – may 2023 MSP430I2040 , MSP430I2041
This command does not read anything related to RTC as there is no RTC in the EVM, yet one of the data read from the meter by this command is the temperature. Hence, this command is considered a command to read the temperature of the EVM using the internal temperature sensor on the MSP430i2040.