SLAA638A august 2014 – may 2023 MSP430I2040 , MSP430I2041
The calibration is defined based on the front-end interface model as shown in Figure 3-1.
For the current design, a two-point calibration and characterization is required. VGAIN, IGAIN, PGAIN, CAP, RES, VDC_OFFSET, IDC_OFFSET are parameters that are calibrated during the process; an estimated value is put into the memory during design and characterization to help speed up calibration.
Default CAP and RES should set to 0 before calibration.
VAC_OFFSET, IAC_OFFSET, PHASE_CORRECT are parameters that may not need calibration but characterization would be sufficient for embedded metering application except for high accuracy of < 0.1%.
The calibration values are written in one flash page in the EVM, thus, when a new value needs to be written the whole page is erased. The provided GUI will do the read, modify and write operation automatically. When using a user-calibration facility, the complete set of calibration values must be read, backed up, modified fields updated and the complete set written back to the EVM.