SLAA870 February 2019 AFE7422 , AFE7444
When frequency hopping to maintain phase continuity, the hop time is an accumulation of the time required to write the 32-bit frequency word plus the time required for the RF output to update after toggling the NCO reset.Figure 10 shows a model scope shot of the theoretical hop time when the SPI is used to reset the NCO.