SLAA871 January 2019 AFE7422 , AFE7444
Figure 19 shows a repeated 120-MHz wideband signal at the output of the repeater without the jammer present. Figure 20 shows the jammer swept from the edge of the effective decimation pass band, through the transition band until the jammer is fully attenuated. The resulting measurement shows –50 dBc of attenuation at 23 MHz, as denoted by marker 2.