SLAA871 January 2019 AFE7422 , AFE7444
Figure 12 shows the setup. Port 1 drives the input of the repeater with frequencies ranging from 1900 MHz to 1920 MHz, and port 2 receives the signals from port 1, documenting the time of flight from Port 1 to Port 2. The average group delay is approximately 1.12 µs. Figure 13 shows a graph of latency as a function of frequencies between 1900 MHz and 1920 MHz.
The maximum gain was determined using the same setup as group delay and is approximately 9 dBm when both of the RX and TX DSA settings are set to 0. Figure 14 shows a graph of gain verses frequencies between 1900 MHz and 1910 MHz.
Figure 12. Latency and Gain Test Setup