SLAA913A January 2020 – June 2021
To allow for accurate comparison between Standby and Sensor Controller system solutions, the HDC2010 sampling code with periodic RF transmission was implemented also on the main Arm Cortex-M4F MCU instead, while the SCE is left unused. Using the same duty-cycle of 60 seconds and same RF parameters and packet length, also the Duty-cycling approach as in the TIDA-00484 reference design was added.