SLAAEB3A May 2023 – July 2024 MSPM0G3507 , MSPM0L1106 , MSPM0L1306
PRODUCTION DATA
Read Current uses the
DirectCommand
function to read the CC2 current value from 0x3A
and return the value. The read-back value is reported in mA.
Table 4-4 shows how to read the 16-bit current measurement from CC2. The current value in the following waveform is 0x00F, which converts to a decimal value of 15mA.
Command | Name | Unit | Type | Description |
---|---|---|---|---|
0x3A | CC2 Current | userA | I2 | 16-bit CC2 current |