SLAAEB8 February   2024 MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1

 

  1.   1
  2. 1Description
  3. 2Required Peripherals
  4. 3Compatible Devices
  5. 4Design Steps
  6. 5Design Considerations
  7. 6Software Flow Chart
  8. 7Application Code
  9. 8Additional Resources
  10. 9E2E

Design Considerations

  1. Input signal bandwidth: The bandwidth of the signal that must be resolved determines the ADC sampling frequency and the amount of data the code must process.
  2. ADC reference voltage: The ADC reference voltage must be selected so the signal amplitude can be fully captured with good resolution.
  3. Filter order: Every increase in filter order is another set of operations the user must perform per each sample. This increases the overall processing time between samples and limits the amount of other processes the user can perform. The result is an increase in filter rejection and increased resolution of the desired signal.