SLAAED9 November 2023 TAA5412-Q1 , TAC5311-Q1 , TAC5312-Q1 , TAC5411-Q1 , TAC5412-Q1
This fault triggers when the absolute value of the difference between the input pins falls under the programmed threshold. This fault is programmable from 0 V to 450 mV in steps of 30 mV. In a typical DC-coupled application, there is a differential DC offset between the input pins from the microphone. This fault can trigger inadvertently in the application if the DC differential is kept below the programmed threshold.