SLAAED9 November 2023 TAA5412-Q1 , TAC5311-Q1 , TAC5312-Q1 , TAC5411-Q1 , TAC5412-Q1
Separate from the overcurrent protection, an internal current sensor monitors the loading on the MICBIAS pin of the device. This feature can be programmed to trigger a fault if the current exceeds the maximum programmed value or falls under the minimum expected load. Note that the programmed threshold is only used for fault detection and does not limit the current supplied by the MICBIAS pin. The high- and low-current thresholds can be programmed from 0 mA to 30 mA (default lower and upper thresholds are 2.6 mA and 18 mA, respectively) with a resolution of 0.117 mA. These thresholds are programmed in DIAG_CFG6 (Page 1, address 0x4C) and DIAG_CFG7 (Page 1, address 0x4D). Since the device is only specified up to 30 mA, the device is not recommended to set the high load current threshold greater than 30 mA.