SLAAEE3A July 2023 – June 2024 MSPM0L1306
The battery running data is input from the GUI for this mode and enables you to run the real test case or evaluate the MSPM0 Gauge with only a launchpad. This method can remove the need of hardware, increase algorithm running frequency and have no limit to the length of battery running data.
To realize this method, first connect the UART COM port and load the MCUData run file in MCU COM Tool. After clicking the data transmit button, wait until the port status changes to “Start transmition!”, shown in Figure 4-13. The data load time and Excel save time is long if the file is very large, about 5 to 10 minutes.
The battery running data is returned from MCU. The benefit of the method is that you can load the battery running data over and over again to improve the algorithm and parameter setting.