SLAAEI4 August 2024 TAC5111-Q1 , TAC5212-Q1 , TAC5311-Q1 , TAC5312-Q1 , TAC5411-Q1 , TAC5412-Q1 , TAD5212-Q1
Figure 4-3 is an example of the BOP algorithm engaging with the following parameters:
Figure 4-4 features an incoming audio signal subject to the parameters of the BOP algorithm. VBAT is dropping from 11V to 10V at the first negative edge of channel two and subsequently the analog output is attenuated to a -3dB signal. As VBAT continues to drop below 10V the output further attenuates to the BOP minimum threshold, a -20dB signal.