SLAAEI4 August 2024 TAC5111-Q1 , TAC5212-Q1 , TAC5311-Q1 , TAC5312-Q1 , TAC5411-Q1 , TAC5412-Q1 , TAD5212-Q1
The release rate is the step rate response when the Distortion Limiter triggers a gain increase. The settling time of the signal is faster as this user-defined rate increases. This threshold is controlled by the coefficient YRAM_REL_COEFFI_LIM. Equation 6 shows how to compute the parameters from the desired attenuation rate in dB/step. The threshold range is from -1x10^6dB/step to 6dB/step and can be programmed in steps of 1x10^-6dB, where RR is the Release Rate of the output signal in dB/step.
Table 3-7 lists the registers corresponding to YRAM_REL_COEFFI_LIM. The default value (0x40BDB7C0) corresponds to 0.1dB/step.
Coefficient | Page | Register | Reset Value | Description |
---|---|---|---|---|
YRAM_REL_COEFFI_LIM | 0x19 | 0x64 | 0x00 | ADC_CH4_SF1_BYT1[31:24] |
YRAM_REL_COEFFI_LIM | 0x19 | 0x65 | 0x00 | ADC_CH4_SF1_BYT2[23:16] |
YRAM_REL_COEFFI_LIM | 0x19 | 0x66 | 0x00 | ADC_CH4_SF1_BYT3[15:8] |
YRAM_REL_COEFFI_LIM | 0x19 | 0x67 | 0x00 | ADC_CH4_SF1_BYT4[7:0] |