SLAAEO3 September   2024 MSPM0L2227 , MSPM0L2228

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction: MSPM0 and LCD End Applications
  5. 2MSPM0 LCD Portfolio
  6. 3Segmented LCD Operation
    1. 3.1 LCD Structure (Simplified)
    2. 3.2 LCD Drive Basics
  7. 4MSPM0 LCD Features
    1. 4.1 Muxing
      1. 4.1.1 Muxing Example
    2. 4.2 Voltage Generation
      1. 4.2.1 Charge Pump
      2. 4.2.2 Contrast Control
    3. 4.3 LCD Clocking
    4. 4.4 LCD Memory and Blinking Mode
      1. 4.4.1 LCD Memory Organization
      2. 4.4.2 Blinking
    5. 4.5 LCD Output Pin Configuration
    6. 4.6 Low Power Mode Feature
  8. 5LCD Layout and Software Considerations
    1. 5.1 LCD Layout Tips
      1. 5.1.1 Hardware-Driven Layout
      2. 5.1.2 Software-Driven Layout
      3. 5.1.3 General Layout Rules
    2. 5.2 LCD Software Tips
      1. 5.2.1 Create a Look-up Table
      2. 5.2.2 Use of #defines
      3. 5.2.3 Efficient Clearing of the LCD Memory
      4. 5.2.4 Double-buffering of the Display Buffer Using Dual Display Memory
  9. 6Additional Resources

Muxing

Segmented LCDs use multiplexing (muxing) to limit control pin count. Types of displays include static (no muxing) and 2 through 8-mux. The notation N-mux means each segment pin Sx drives N segments on the display – this also means there are N common (COMx) pins. Each LCD segment on the display is driven by the combination of a COMx pin and Sx pin, providing a difference in potential across the liquid crystals for that segment.

Muxing allows a limited number of pins to control a larger number of segments. If there is an 8-mux LCD display, then there are 8 COM pins and each segment (Sx) pin drives 8 segments. So when using an 8-mux capable MSPM0 with 51 Sx pins available (S0-S50), then MSPM0 is able to control 408 segments with only 8 (COMx) + 51 (Sx) = 59 pins.

MSPM0 devices with 8-mux mode support up to 408 segment displays. However, make sure to check the device-specific data sheet to see how many segments the particular device supports, the number of supported segments is limited not only by the muxing capability of the LCD module, but also by the number of LCD pins available on the particular device in a particular pin-package.

MSPM0L222x MUX Configurations Figure 4-1 MUX Configurations