SLAU131Y October 2004 – June 2021
The linker supports a special copy table name, BINIT (or binit), that you can use to create a boot-time copy table. This table is handled before the .cinit section is used to initialize variables at startup. For example, the linker command file for the boot-loaded application described in Section 9.9.2 can be rewritten as follows:
SECTIONS
{
.flashcode: { app_tasks.c.obj(.text) }
load = FLASH, run = PMEM,
table(BINIT)
...
}
For this example, the linker creates a copy table that can be accessed through a special linker-generated symbol, __binit__, which contains the list of all object components that need to be copied from their load location to their run location at boot-time. If a linker command file does not contain any uses of table(BINIT), then the __binit__ symbol is given a value of -1 to indicate that a boot-time copy table does not exist for a particular application.
You can apply the table(BINIT) specification to an output section, GROUP, or UNION member. If used in the context of a UNION, only one member of the UNION can be designated with table(BINIT). If applied to a GROUP, then none of that GROUP's members may be marked with table(BINIT).The linker detects violations of these rules and reports them as warnings, ignoring each offending use of the table(BINIT) specification.