SLAU132Y September 2004 – June 2021
The compiler supports the 2011 standard of C as standardized by the ISO. However, in addition to the list in Section 6.16.1, the following run-time functions and features are not implemented or fully supported in C11 mode: