SLAU144K December 2004 – August 2022 MSP430AFE221 , MSP430AFE222 , MSP430AFE223 , MSP430AFE231 , MSP430AFE232 , MSP430AFE233 , MSP430AFE251 , MSP430AFE252 , MSP430AFE253 , MSP430F2001 , MSP430F2002 , MSP430F2003 , MSP430F2011 , MSP430F2012 , MSP430F2013 , MSP430F2101 , MSP430F2111 , MSP430F2112 , MSP430F2121 , MSP430F2122 , MSP430F2131 , MSP430F2132 , MSP430F2132-EP , MSP430F2232 , MSP430F2234 , MSP430F2252 , MSP430F2252-Q1 , MSP430F2254 , MSP430F2272 , MSP430F2272-Q1 , MSP430F2274 , MSP430F2274-EP , MSP430F233 , MSP430F2330 , MSP430F235 , MSP430F2350 , MSP430F2370 , MSP430F2410 , MSP430F2416 , MSP430F2417 , MSP430F2418 , MSP430F2419 , MSP430F247 , MSP430F2471 , MSP430F248 , MSP430F2481 , MSP430F249 , MSP430F2491 , MSP430F2616 , MSP430F2617 , MSP430F2618 , MSP430F2619 , MSP430G2001 , MSP430G2101 , MSP430G2102 , MSP430G2111 , MSP430G2112 , MSP430G2121 , MSP430G2131 , MSP430G2132 , MSP430G2152 , MSP430G2153 , MSP430G2201 , MSP430G2201-Q1 , MSP430G2202 , MSP430G2203 , MSP430G2210 , MSP430G2211 , MSP430G2212 , MSP430G2213 , MSP430G2221 , MSP430G2230 , MSP430G2231 , MSP430G2231-Q1 , MSP430G2232 , MSP430G2233 , MSP430G2252 , MSP430G2253 , MSP430G2302 , MSP430G2303 , MSP430G2312 , MSP430G2313 , MSP430G2332 , MSP430G2333 , MSP430G2352 , MSP430G2353 , MSP430G2402 , MSP430G2403 , MSP430G2412 , MSP430G2413 , MSP430G2432 , MSP430G2433 , MSP430G2444 , MSP430G2452 , MSP430G2453 , MSP430G2513 , MSP430G2533 , MSP430G2544 , MSP430G2553 , MSP430G2744 , MSP430G2755 , MSP430G2855 , MSP430G2955 , MSP430TCH5E
* INCD[.W] | Double-increment destination | |
* INCD.B | Double-increment destination | |
Syntax |
INCD dst
or
INCD.W dst | |
INCD.B dst | ||
Operation | dst + 2 → dst | |
Emulation |
ADD #2,dst | |
ADD.B #2,dst | ||
Description | The destination operand is incremented by two. The original contents are lost. | |
Status Bits | N: | Set if result is negative, reset if positive |
Z: | Set if dst contained 0FFFEh, reset otherwise | |
Set if dst contained 0FEh, reset otherwise | ||
C: | Set if dst contained 0FFFEh or 0FFFFh, reset otherwise | |
Set if dst contained 0FEh or 0FFh, reset otherwise | ||
V: | Set if dst contained 07FFEh or 07FFFh, reset otherwise | |
Set if dst contained 07Eh or 07Fh, reset otherwise | ||
Mode Bits | OSCOFF, CPUOFF, and GIE are not affected. | |
Example | The item on the top of the stack (TOS) is removed without using a register. |
.......
PUSH R5 ; R5 is the result of a calculation, which is stored
; in the system stack
INCD SP ; Remove TOS by double-increment from stack
; Do not use INCD.B, SP is a word-aligned register
RET
Example | The byte on the top of the stack is incremented by two. |
INCD.B 0(SP) ; Byte on TOS is increment by two