2.4 Revisions
The first production revision of the LaunchPad development kit in 2010 was 1.3. In 2012 the LaunchPad board revision changed from 1.4 to 1.5 to align with the new release of Value Line devices. The differences in the schematic and the kit contents are:
- Layout and Schematic:
- Voltage feedback in the emulator changed to increase startup stability (Rev 1.3 to Rev 1.4)
- Rearranged jumper J3 to support two UART configurations: vertical (SW UART), horizontal (HW UART)
- VCC on the connector J4 can now be disconnected from the emulator VCC by J3
- Pullup resistor R34 and capacitor C24 on P1.3 removed to reduce the current consumption
- Presoldered male headers J1 and J2