SLAU319AF July 2010 – September 2022
CKL, CKH
CRC checksum high and low bytes. The checksum is computed on bytes in BSL core command section only. The CRC is computed using the MSP430F5xx CRC module specification (see the CRC chapter of the MSP430F5xx and MSP430F6xx Family User's Guide for implementation details).
NL, NH
Number of bytes in BSL core data packet, broken into high and low bytes.
ACK
Sent by the BSL after the packet is received to acknowledge receiving the data correctly. This does not imply the BSL core data is a correct command or that it was executed correctly. ACK signifies only that the packet was formatted as expected and had a correct checksum.
If the PI encounters an error at any stage of receiving the packet, it immediately responds with the appropriate error message.