SLAU319AF July 2010 – September 2022
To protect data within the device, most core commands are protected. A protected command is successfully complete only after the device has been unlocked by sending the RX Password command with the correct password. In addition, commands specific to the peripheral interface are not protected.
Unprotected Commands
RX Password
Mass Erase
Password Protected Commands
RX Data Block to Address (flash or RAM)
TX BSL Version
TX Data Block
Erase Segment
Erase Bank
Set Program Counter
Toggle INFO_A Lock
Erase Main
CRC Check