SLAU533D September 2013 – April 2017
The F5529 LaunchPad development kit comes programmed with an out-of-box demonstration example. Let's get started!
This section only describes how to use the demo. More details about the F5529 LaunchPad development kit are given later.
The demo works on a Windows PC, Linux PC, or Mac. It requires that (at minimum) the power jumpers (3.3 V and 5 V) on the isolation jumper block be connected. These supply power to the target F5529 device. As shipped from TI, these jumpers are connected.