4 Hardware Installation
This section describes how to install the drivers for all MSP debug probes. The drivers are needed to enable the IDE (integrated development environment) to use the debug probe that is connected to the system. There are four different ways to install the drivers.
- CCS desktop: During the CCS setup, all MSP debug probe drivers are installed for all supported operation systems.
- CCS cloud: The automatic driver installer is included in the TI Cloud Agent application, which must be downloaded when connecting a local MSP debug probe to CCS cloud.
- Stand-alone driver installer: The stand-alone driver installer is available only for Windows. It installs all MSP debug probe drivers.
- Using another supported IDE such as IAR EW430 or the MSP-Flasher: During the setup, all MSP debug probe drivers are installed.