SLAU647O July 2015 – April 2020
The MSP-FET430UIF is a powerful debug probe for application development on MSP430 microcontrollers. This is a legacy debugger being replaced by MSP-FET.
The MSP-FET430UIF provides a USB interface to program and debug the MSP430 MCUs in-system through the JTAG interface or the pin-saving Spy-Bi-Wire (2-wire JTAG) protocol.
The MSP-FET430UIF development tool supports development with all MSP430 MCUs and is designed for use with PCBs that contain MSP430 MCUs; for example, the MSP430 target socket boards.
Two different version of the MSP-FET430UIF are available, version 1.3 and version 1.4a. There are limitations when using version 1.3. See Section 5.7.1 for more details.