SLAU647O July 2015 – April 2020
The MSP-FET supports two different Backchannel UART modes, one with flow control and one without. The different modes can be selected by opening the corresponding COM port with a dedicated baud rate. See Table 5 for the specific baud rates for each command.
NOTE
The baud rates used by these activation commands cannot be used for communication.
NOTE
TheBackchannel UART is disabled until the COM port is opened with a valid baud rate.
If none of the specified commands are transferred before setting the communication baud rate, communication starts with the default settings: 3.3-V target VCC, no flow control mechanism, no parity.