SLAU664B February 2016 – August 2017
IAR Embedded Workbench for MSP430 is another very powerful integrated development environment that allows you to develop and manage complete embedded application projects. It integrates the IAR C/C++ Compiler, IAR Assembler, IAR ILINK Linker, editor, project manager, command line build utility, and IAR C-SPY® Debugger.
Learn more about IAR Embedded Workbench for MSP430 and download it at supp.iar.com/Download/SW/?item=EW430-EVAL.
IAR 6.10 or higher is required. To open the demo in IAR, click File>Open>Workspace…, and browse to the *.eww workspace file inside the \IAR subdirectory of the desired demo. All workspace information is contained within this file.
The subdirectory also has an *.ewp project file. This file can be opened into an existing workspace by clicking Project>Add-Existing-Project….
Although the software examples have all of the code required to run them, IAR users may download and install MSPWare software, which contains MSP430 MCU libraries and the TI Resource Explorer. These are already included in a Code Composer Studio IDE installation (unless the user selected otherwise).