SLAU678C March 2016 – November 2022
Software examples are included with the MSP430FR5994 LaunchPad development kit (see Table 3-1), and can be found in the MSP430FR5994 LaunchPad development kit Download Page and are also available in MSP430Ware for MSP Microcontrollers.
Demo Name | BoosterPack Required | Description | More Details |
---|---|---|---|
OutOfBox_FR5994 | None | The out-of-box demo pre-programmed on the LaunchPad from the factory. Demonstrates features of MSP430FR5994 MCU. | Section 3.1 |
BlinkLED_FR5994 | None | Blinks an LED on the LaunchPad at a fixed interval. | Section 3.2 |
BOOSTXL-AUDIO_ RecordPlayback_ MSP430FR5994 |
| Demonstrates how to record and playback audio from FRAM memory using DMA. | Section 3.3 |
BOOSTXL-AUDIO_ LEA_MSP430FR5994 |
| Demonstrates the performance of the MSP low-energy accelerator (LEA) by performing FFT and FIR. | Section 3.4 |
EEPROM Emulation reference design |
| Emulates EEPROM using FRAM technology on MSP supporting both I2C and SPI | Section 3.5 |
To use any of the software examples with the LaunchPad kit, you must have an integrated development environment (IDE) that supports the MSP430FR5994 MCU. Table 3-2 lists the minimum requirements for IDEs.
Code Composer Studio™ IDE | IAR Embedded Workbench® IDE |
---|---|
Code Composer Studio IDE v6.1.3 or later | IAR Embedded Workbench for MSP430 v6.40.2 or later |
For more details on how to get started quickly, and where to download the latest Code Composer Studio and IAR Embedded Workbench IDEs, see Section 4.