SLAU723A October 2017 – October 2018 MSP432E401Y , MSP432E411Y
As shown in Figure 20-13, the pixel data stored in frame buffers go through palette (if applicable) and grayscaler and serializer before reaching the output FIFO. As a result, it is likely that the data fed to the output FIFO is numerically different from the data in the frame buffers. (However, they represent the same color or grayscale.)
The output FIFO formats the received data according to display modes. Figure 20-13, shows the actual data output on the external pins.