SLAU802 March 2019
The LP-MSP430FR2476 provides an external clock in addition to the internal clocks in the device.
The 32.768-kHz crystal allows for lower LPM sleep currents than do the other low-frequency clock sources. Therefore, the presence of the crystal allows the full range of low-power modes to be used.
The internal clocks in the device default to the following configuration:
For more information about configuring internal clocks and using the external oscillators, see the MSP430FR4xx and MSP430FR2xx Family User's Guide.