To connect the GUI to the SCB and
update the firmware, follow these steps:
- Setup and launch the GUI as
described in the EVM specific user's guide.
- With the EVM plugged in, after
launching the GUI, close the README.md file page to initiate the connection. If
successful, "Hardware Connected" should be visible near the bottom left corner
of the GUI as shown in Figure 3-2.
- A green indicator with
the device type and the text "DEVICE CONNECTED" should also be visible
near the top left of the GUI, as shown in Figure 3-3.
- If you receive a pop up message
asking you to update the firmware, do so.
- It is possible that this
fails the first time if the SCB didn't properly connect first. In this
case, just connect to the GUI following the steps below before updating
the firmware.
- If "Hardware Connected" and
"DEVICE CONNECTED" do not show in the GUI, it is possible that the SCB is
already in Devce Firmware Update (DFU) mode. If so, then the Program
Device... button under File >> Program Device... will not
be grayed out. Click the button to begin the firmware update.
- You may need to close
another popup message or so letting you know that the GUI couldn't
connect to the SCB.
- If the firmware fails to
update, try the same connectivity steps outlined in step 5.c.
- If the Program Device...
button is grayed out, then the device is not in DFU mode. In this case, try to
connect the GUI to the SCB by doing any of the following:
- Press the
(connect) symbol in the bottom left
corner.
- Check different hardware
COM ports under Options >> Serial Port, as shown in Figure 3-4.
- If neither of those work,
many connectivity issues can be addressed by doing one of the
following:
- Long-press the
RESET button on the SCB with the EVM and SCB connected to each
other.
- Refresshing the GUI can also sometimes help.
- Connect the SCB
using a different USB port.
- Avoid
using long cables and USB hubs.
- If using
a desktop PC, try a USB port on the back.
- If the hardware still
does not connect, you may need to update the firmware manually, as
described in Section 3.2.3.1.
- After the SCB has connected to
the GUI, update the firmware by going to File >> Program Device...,
as shown in Figure 3-5.
- If the firmware fails to
update, try the same connectivity steps outlined in step 5.c.
- If the Firmware still
fails to update, you may need to update the firmware manually, as
described in Section 3.2.3.1.
- Once the firmware has been
updated, the SCB can be used with the EVM and GUI per the EVM-specific user's
guide.