SLAU846A June 2023 – October 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
In FULL channels, the DMA controller has two extended modes selected by the DMAEM bits as listed in Table 4-3. Each channel is individually configurable for the extended mode. For example, channel 0 can be configured in table mode while channel 1 is configured in fill mode.
DMAEM | Extended Mode | Description |
---|---|---|
00 , 01 | Normal mode | Operation is defined by DMATM |
10 | Fill mode | Used to fill predefined data patterns into memory |
11 | Table mode | Used to help configure a table of peripheral control registers |