SLAU846A June 2023 – October 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
The VREF module for the MSPM0Gxx family is a shared voltage reference module which can be leveraged by a variety on on-board analog peripherals. VREF allows users to choose between using an internally generated reference voltage or using an externally provided reference voltage from outside the MCU.
The VREF module features include:
Figure 15-1 shows the block diagram of the VREF module.