SLAU846A June 2023 – October 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
The execution time of the BCR can be reduced by enabling fast boot mode. Fast boot mode, when enabled, speeds up the boot process using the following methods:
To enable fast boot mode, set the fast boot mode to enabled in the BOOTCFG2.FASTBOOTMODE field in the NONMAIN flash memory.