SLAU846B June 2023 – November 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3519
9-bit mode is enabled by setting MODE bit to ADDR9BIT in the UARTx.CTL0 register. This feature is useful in a multi-drop configuration of the UART where a single controller connected to multiple peripherals can communicate with a particular peripheral through its address or set of addresses along with a qualifier for an address byte. In 9-bit UART mode, the parity enable/mode bits are ignored and the UART word length (UARTx.LCRH.WLEN) must be set to 8 bit.
Receive Transaction:In 9-bit mode, a peripheral checks for the address qualifier at the location of the parity bit. If set, the received byte is compared with the preprogrammed address in UARTx.ADDR register:
The address can be predefined in the UART.ADDR register to match with the received byte. The matching can be extended to a set of addresses using the address mask in the UART.AMASK register. By default, the UART.AMASK is 0xFF, meaning that only the specified address must match
Transmit Transaction:
All the send transactions in 9-bit UART mode are interpreted as:In 9-bit mode, the 9th bit can be controlled by software. The EPS bit setting of the LCRH register reflects the 9th bit for transmit transactions. To indicate an address byte, the software must set the EPS bit before the byte transmission. For data byte transmissions, the EPS bit must be cleared before the byte transmission. For a complete transmit transaction, the address byte must be transmitted as a single byte transaction with EPS bit set, followed by a data byte burst with EPS bit cleared.
9th bit handling:
PEN | SPS | EPS | 9th Bit (Transmitted or Verified) |
---|---|---|---|
0 | X | X | Not transmitted or verified |
1 | 1 | 0 | 0 (= Data) |
1 | 1 | 1 | 1 (= Address) |