SLAU846B June 2023 – November 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3519
The DAC module provides different interrupt sources which can be configured to source the DMA trigger. In order of decreasing interrupt priority, the DMA trigger events from the DAC are given as the following table. When the DMA channel is needed by the DAC, the DMA trigger should be unmasked in the IMASK register.
To configure the DMA controller to trigger from the DAC, please see Section 16.2.8.
Index (IIDX) | Name | Description |
---|---|---|
0x0 | NO_INTR | No bit set (IIDX.STAT = 0) means there is no pending interrupt request |
0x2 | MODRDYIFG | Module ready interrupt once DAC is enabled and DAC output is settled |
0x9 | FIFOFULLIFG | FIFO full interrupt flag is set when the FIFO is full |
0xA | FIFO1B4IFG | FIFO one fourth empty interrupt flag is set when one fourth of FIFO locations are empty. |
0xB | FIFO1B2IFG | FIFO half empty interrupt flag is set when half of the FIFO locations are empty. |
0xC | FIFO3B4IFG | FIFO three fourth empty interrupt flag is set when all the locations in FIFO are empty. |
0xD | FIFOEMPTYIFG | FIFO empty interrupt flag is set when all data in the FIFO have been shifted out. |
0xE | FIFOURUNIFG | FIFO underrun flag is set when the FIFO read trigger is asserted while the FIFO is empty. |
0xF | DMADONEIFG | DMA done interrupt flag is set when the DMA data transfer of programmed block size is completed |