SLAU846B June 2023 – November 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3519
The input select bits TIMx.IFCTL_xy[0/1].ISEL select the input source to the filter input as the corresponding CCP input, CCP0 for cross-triggering across CC blocks, an external trigger, XOR (used in Hall input mode), event subscribers, or comparator inputs.
Input selection (TIMx.IFCTL_xy[0/1].ISEL) | Source |
---|---|
0h | TIMx CCP of the corresponding capture compare unit |
1h | Input pair CCPx of the capture compare unit. [CCP0/CCP1, CCP2/CCP3] |
2h | TIMx CCP0 |
3h | Cross trigger signal |
4h | XOR of CCP inputs. Used in Hall input mode. See Section 27.2.3.1.4 |
5h | Subscriber event 0 (FSUB0). See Section 27.2.9.2 |
6h | Subscriber event 1 (FSUB1). See Section 27.2.9.2 |
7h | COMP0_OUT (devices with comparator only) |
8h | COMP1_OUT (devices with comparator only) |
9h | COMP2_OUT (devices with comparator only) |