SLAU846B June 2023 – November 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3519
There are two settings for the CCP output channel behavior in a fault condition, TIMA.CCACT_01[0/1].FEXACT (fault exit behavior) and TIMA.CCACT_01[0/1].FENACT (fault entry behavior). The output behavior of fault condition is described in Table 27-22.
Bit Fields | Output Behavior | |
---|---|---|
FEXACT | FENACT | |
0 | The CCP output value is unaffected by the fault event | |
1 | CCP output value is set high | |
2 | CCP output value is set low | |
3 | CCP output value toggles | |
4 |
CCP output is tristated (Hi-Z) |
If using the TIMA_FALx pin with the CCP capture channel inputs (such as adding deadband to complimentary PWMs) for low latency actions, an external connection should be in hardware between the TIMA_FALx pin and TIMAx_Cy pin (x = timer instance, y = CC channel).