SLAU846B June 2023 – November 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3519
One can configure the SPI to be controller mode by setting the CTL1.MS bit to 1, and in peripheral mode by clearing the CTL1.MS bit.
The CTL0.CSSEL bit selects which connected peripheral is addressed by the up to 4 CS signals. The bits are controlled by the SPI module in controller or target/peripheral mode. The selected signal is controlled during the transfers.
The chip select signal needs to be provided by the controller in four-wire mode and the chip select polarity can be inverted by configuring the PINCM.CSx.INV register.
In peripheral mode, the clock is provided by the controller and used by the peripheral to capture the data. The peripheral has the option to operate in 3-wire or 4-wire mode. 4-wire mode only accepts data transfers if the CS is activated.
When the CTL0.CSCLR bit is set, the transmit/receive shift register counter is cleared automatically when the CS goes to the inactive state. When using the Motorola 4-wire or National Microwire mode, follow these constraints:
Following these constraints helps the peripheral to synchronize again on the controller in case of a disturbance or glitch on the clock line or during initialization. This bit is relevant only in the peripheral mode.