SLAU846B June 2023 – November 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3519
Sampled mode is a method of operation for the comparator, which compares input signals at discrete time intervals or samples, producing output signals that change only at the sampling points. The SAMPMODE bit in the register CTL2 enables or disables the sampled mode.
To define the sampling window, two events, EVT0 and EVT1, are generated from the timer. The sampling window can be aligned to less noisy phases with the use of these events. EVT0 sets the sampling window, while EVT1 clears it.
In sampled mode, the output of the comparator is captured only when the sampling window is high, and the output is not captured at other times. The captured output is used for interrupt and event generation.
By using sampled mode, the comparator can reduce the effects of noise in the input signals, resulting in more accurate and reliable comparisons. The use of EVT0 and EVT1 to define the sampling window allows for greater flexibility in aligning the window to the least noisy phases of the input signals, further improving the accuracy of the comparisons.
Please note following when internal DAC8 is used in sampled mode and user wants to enter Standby0 mode; for comparator output to work as expected, it is to be ensured that COMP is ready by polling the OUTRDYIFG flag before SoC enters Standby0 mode.
User can follow the below sequence for this scenario.